Other Parts Discussed in Thread: TMS320DM6446
Hi,
I am trying to connect to a DM6446 with XDS560 PCI emulator. I am using CCS 4.1.2.00027. I created a target launch configuration with the default settings for XDS560 PCI and TMS230DM6446 board type. On trying to launch the configuration I get the following error.
Exception occurred during launch.
Reason : Failed to initialize Debug Server
Reason : Can't generate board data file C:\Program Files\Texas Instruments\ccsv4\DebugServer\bin\win32\BrdDat\ccBoard0.dat
The device name has invalid spelling.
It must have an alphabetic first character.
It must use only alphanumeric or underscore characters.
Any idea what could be going wrong? I could connect to a EVMDM642 board with the default configs.
Thanks
===========================
The .ccxml file in use is as follows
<?xml version="1.0"
encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Texas Instruments XDS560 PCI
Emulator_0">
<instance XML_version="1.2" desc="Texas Instruments XDS560
PCI Emulator_0" href="connections\TIXDS560_Connection.xml" id="Texas
Instruments XDS560 PCI Emulator_0" xml="TIXDS560_Connection.xml"
xmlpath="connections"/>
<connection XML_version="1.2" id="Texas Instruments XDS560
PCI Emulator_0">
<instance XML_version="1.2"
href="drivers\tixds560icepick_c.xml" id="drivers"
xml="tixds560icepick_c.xml" xmlpath="drivers"/>
<instance XML_version="1.2"
href="drivers\tixds560arm9.xml" id="drivers" xml="tixds560arm9.xml"
xmlpath="drivers"/>
<instance XML_version="1.2"
href="drivers\tixds560etb11.xml" id="drivers" xml="tixds560etb11.xml"
xmlpath="drivers"/>
<instance XML_version="1.2"
href="drivers\tixds560c64xp.xml" id="drivers" xml="tixds560c64xp.xml"
xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="TMS320DM6446_0"
href="Devices\dm6446.xml" id="TMS320DM6446_0" xml="dm6446.xml"
xmlpath="Devices"/>
</platform>
</connection>
</configuration>
</configurations>