Other Parts Discussed in Thread: AM3352
Dear support,
I am debugging an application on a AM3352 device with the SDK "ti-processor-sdk-linux-am335x-evm-01.00.00.00" and the CCS 6.1.2.00015.
My code links a static library (.a) which is compiled in debug mode. When I debug my code I can step into the functions of the lib.
If I put a breakpoint on the functions of my code and go with a run (F8), the debugger stops on the breakpoints as expected.
But it does not stop on the breakpoints I put on the source code of the library.
A difference I noticed is that, on the Break Point View, the BP on my code are showed with the line number (e.g. ermes.c [line: 3192] ) while the BP on the lib are marked as SW BP (e.g. media.c, line 94 [S/W BP] ) .
How can I stop automagically on these last BP?
Thank you.