This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 6.1.1.00022 only recognizes one version of GCC compiler (the oldest)

After updating GCC compiler, which installed gcc_msp430_4.9.14r1_364,

project include files and tools still point to older gcc_msp430_4.9.14r1_167.

(Yes I have rebooted PC and restarted CCS)

Menu Window->Preferences->Code Composer Studio->Build->Compilers

only lists one GCC version available:

GNU v4.9.1 (Red Hat) [C:/ti/ccv6/tools/compiler/gcc_msp430_4.9.14r1_167]

Pressing the Refresh button on this screen did not help.

 

My workaround was to exit CCS, go to C:/ti/ccv6/tools/compiler/ and drag the gcc_msp430_4.9.14r1_167 folder out to the desktop.

Startup CCS again and now all project references point to the newer

gcc_msp430_4.9.14r1_364 folder.

 

It appears that the two versions can not co-exist.

 

I am running Windows 8.1 64-bit environment if that matters.