This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem running C6000 Linker from the command line

In order to test running the linker from the command line, I have successfully created a new project using the CCS IDE v 6.1.1.00022 (File->New->CCS Project) and would now like to run the linker CL6x.exe from the command line to link the object code generated by the compiler .  I copied the linker command file generated by default c6748.cmd, to the debug directory and added one line to the .cmd file main.obj.

When I run the linker using Cl6x --run_linker c6748.cmd

I get "error: no input section is linked in"

if it bypass the cmd file and just run Cl6x --run_linker main.obj" I get the same error.

How can I use the IDE to generate the .obj files and then use the linker from the command line to successfully generate the same .out file as the IDE created.  I thought I could just add the .obj file to the .cmd file but I am missing something.