This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv6.1.1: Where is bug Tracking ID: SDSSCM00051261

Guru 20075 points

Hello,

Way back on Dec 9, 2014 I posted an issue with not being able to get exception handling to work for c files (when treat c files as c++ files is selected).

See e2e.ti.com/.../387043

A bug report was filed (Tracking ID: SDSSCM00051261), but that bug # has seemed to disappear from bug tracking.

What happened to that bug?

Stephen

  • Hi Stephen,
    The bug is still there (and fixed in 6.2.11). I see that when I gave the bug ID, I had a typo. Use the below ID (with one less "S")

    SDSCM00051261

    Thanks
    ki
  • There were several bugs reported in that post.

    The bug described in SDSCM00051261 was for "The exception handling (_eh) version of runtime library is not automatically built when --exceptions option is enabled"

    Did You file the bug that related to "Enable C++ exception handling" not getting enabled when "Treat C files as C++ files" is enabled?

    Thanks,

    Stephen