This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI DSP lib performance improved after using fixed input value

Hello everyone

When I use the function "DSPF_sp_dotp_cplx" from TI DSP library 3.4 on C6678, I found that the elapsed cycles can be reduced by using the fixed value. 

The definition of function is: void DSPF_sp_dotp_cplx(const float * x, const float * y, int nx, float * restrict re, float * restrict im);

* @param x Pointer to array holding the first floating-point vector
* @param y Pointer to array holding the second floating-point vector
* @param nx Number of values in the x and y vectors
* @param re Pointer to the location storing the real part of the result
* @param im Pointer to the location storing the imaginary part of the result

If I use predefined value for "nx" as input, the performance of function can be increased by 24%~28%. For example:

If I use the function like this: DSPF_sp_dotp_cplx(ptr_x1, ptr_x2, 32, re_opt, im_opt);

The elapsed cycles is 93

If I use the function like this: n= 32; DSPF_sp_dotp_cplx(ptr_x1, ptr_x2, n, re_opt, im_opt); 

the elapsed cycles is 129.

When n=64. the cycles of fixed value scenario is 133. Another scenario is 176.

I had check the assemble file. I did not see different between two files. Can you tell me how the performance can be improved by using predefined value?

I set opt_level at 3, opt_for_space at 1, and --symdebug:none

Thanks

Xining Yu