Hi,
first I want to say that the (floating) license system is a s***, f***, *** system
I'm absolutly not amused, to spend two hours of my time for such a system.
First you have to grap the software from different sites read the documentation (of the license system), install and try to run the license server,
and in the end it is not running.
I don't want to know how it works in detail, I only want to link my code.
But the Code Composer only says "exceeds code size limit", but it is always able to get one of the important "CCS_DEBUGGER" licenses at startup,
but it never gets one of the "CCS_LINKER_FULL" licenses.
The CCS shows that it is licensed in the window title bar, but from where or so you can only guess, or if the connection to the server fails, is used or is ignored.
Thanks for such a good system