This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error in Soc Analyzer Setup

Hi, all

 

I'm using DM6467 EVM.

 

I followed the soc analyzer instruction at wiki.

When I tried to set up webser, following error occurred.

I tried to "alias ipv6 off" in "/etc/modprobe.conf". But it didn't work. The error was still ther.

 

Any idea?

 

BTW, I think the soc analyzer help is a bit confusing.

It says "copy encodeCombo.x64p, decodeCombo.x64p, loopbackCombo.x64p". But what application should run on target correspondingly?

encode for encodeCombo.x64p?

decode for decodeCombo.x64p?

thanks.

==============================================================

root@192.168.2.221:/opt/dvsdk/dm6467/web# ./thttpd -c "/cgi-bin/*"
ipv6: disagrees about version of symbol struct_module
modprobe: FATAL: Error inserting ipv6 (/lib/modules/2.6.10_mvl401-davinci_evm-PS
P_01_30_00_082/kernel/net/ipv6/ipv6.ko): Invalid module format

root@192.168.2.221:/opt/dvsdk/dm6467/web# ipv6: disagrees about version of symbo
l struct_module
modprobe: FATAL: Error inserting ipv6 (/lib/modules/2.6.10_mvl401-davinci_evm-PS
P_01_30_00_082/kernel/net/ipv6/ipv6.ko): Invalid module format

=============================================================