This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

New CCS needs new compiler? Where is ARM compiler version 5.2.6?

I had CCS 6.1.1. I recently installed the newer CCS 6.1.2. Now I am getting this message. Do I need to install the new compiler? Where do I get it from?

Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed: 5.2.6 [ARM]. Another version of the compiler will be used during build: 5.2.5. Please go to <a href="liveaction:OpenAppCenter">CCS App Center</a> to install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties. EQU_Firmware_L0 properties Problems

Thank you.

Jonathan