This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debugger Initialization Error for Code Composer Studio Version 6.1.2

I just installed Code Composer Studio newest version which is 6.1.2 on my XP Windows system Service Pack 2.


When I try to debug a program I get a popup window that says:

"Debugger Initialization Error"

and the main message is:

"Unable to load ../../../emulation/tpi/tpiarm_x.dll: The specified procedure could not be found."

When I use the dependency walker program from Microsoft to look at tpiarm_x.dll I see that the "KERNEL32.DLL" file is red which indicates that it contains an unresolved C function which is "GetLogicalProcessorInformation".  The parent DLL is "MSVCR120.DLL".

I also get  the following error message displayed at the bottom which is:
"Error: At least one module has an unresolved import due to a missing export function in an implicitly dependent module."

According to information shown in the "Add/Remove Files program" under the windows Control Panel I have the following Microsoft VC++ Redistributables already installed:

2005, 2008, 2010, 2012, and 2013.

Can anyone help me with this problem?

I think I may need to install some upgrade or patch.

Thanks,