Other Parts Discussed in Thread: OMAP3530, OMAP-L138
Hi All.
I am using a CCS4 and XDS510 USB+ to connect to a Beagleboard.
At first, I was not able to connect to ARM side of the Beagleboard. But after I went through http://e2e.ti.com/support/dsp/omap_applications_processors/f/447/t/29982.aspx?PageIndex=1 and removed the .gel files. I was then able to connect to the ARM. However, I was still receiving error message for DSP side. And then I went through http://processors.wiki.ti.com/index.php/Debugging_the_DSP_side_of_a_DSPLink_application_on_OMAP_using_CCS and changed the examples as mentioned. I was then able to connect to DSP side. Then when I try to load my program from menu->Target->load program, I have been getting the following message. I am not able to load my code which is different than the example code used to remove the DSP from reset mode and connect the CCS to it. I need a help on this ASAP.
Thanks,
Pramod
Trouble Writing Memory Block at 0x82805a80 on Page 0 of Length 0x104:
Error 0x00000006/-1060
Error during: Memory, Register,
An unknown error prevented the emulator from accessing the processor
in a timely fashion.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.