hi all......
#10010 errors encountered during linking; "I Remember demo.out" not built
#10099-D program will not fit into available memory. placement with alignment fails for section ".cinit" size 0xa1 . Available memory ranges:
This was my first issue so change the flash size to FLASH : origin = 0xb000, length = 0x4FE0 from FLASH : origin = 0xc000, length = 0x3FE0
then this issue solved, but when i try to debug getting error " data verification error occurred, file load failed. " shown below,
MSP430: File Loader: Data verification failed at address 0x0000B000 Please verify target memory and memory map.
MSP430: GEL: File: E:\Sai\workspace_v6_0 msp430\I Remember demo\Debug\I Remember demo.out: a data verification error occurred, file load failed.
here is my SYSTEM MEMORY MAP
/****************************************************************************/
/* SPECIFY THE SYSTEM MEMORY MAP */
/****************************************************************************/
MEMORY
{
SFR : origin = 0x0000, length = 0x0010
PERIPHERALS_8BIT : origin = 0x0010, length = 0x00F0
PERIPHERALS_16BIT : origin = 0x0100, length = 0x0100
RAM : origin = 0x0200, length = 0x0200
INFOA : origin = 0x10C0, length = 0x0040
INFOB : origin = 0x1080, length = 0x0040
INFOC : origin = 0x1040, length = 0x0040
INFOD : origin = 0x1000, length = 0x0040
FLASH : origin = 0xc000, length = 0x3FE0
INT00 : origin = 0xFFE0, length = 0x0002
INT01 : origin = 0xFFE2, length = 0x0002
INT02 : origin = 0xFFE4, length = 0x0002
INT03 : origin = 0xFFE6, length = 0x0002
INT04 : origin = 0xFFE8, length = 0x0002
INT05 : origin = 0xFFEA, length = 0x0002
INT06 : origin = 0xFFEC, length = 0x0002
INT07 : origin = 0xFFEE, length = 0x0002
INT08 : origin = 0xFFF0, length = 0x0002
INT09 : origin = 0xFFF2, length = 0x0002
INT10 : origin = 0xFFF4, length = 0x0002
INT11 : origin = 0xFFF6, length = 0x0002
INT12 : origin = 0xFFF8, length = 0x0002
INT13 : origin = 0xFFFA, length = 0x0002
INT14 : origin = 0xFFFC, length = 0x0002
RESET : origin = 0xFFFE, length = 0x0002
}
Thanks,