Other Parts Discussed in Thread: TM4C123GH6PGE
Hi
When I'm installing CCSv5 on Win10, Win10 does not support this.
Can't I use CCSv5 on Win10?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TM4C123GH6PGE
Hi
When I'm installing CCSv5 on Win10, Win10 does not support this.
Can't I use CCSv5 on Win10?
Thank you for replying.
I have only board TM4C123GH6PGE, and enclosed USB.
And, in USB, there are only CCSv5 install file.
If I want to run CCS on Win10 normally, do I have to buy new board and CCSv6?
Is there any solutions that I can run CCS on Win10 normally, with these situaitons?
I don't have TM4C board, but I have the same experience on F28069M LaunchPad.
In my case, when the LaunchPad is connected, the on-board XDS100v2 Channel B is not shown. The is due to the driver configuration. I have to launch the "Device Manager" program of Windows 10. Under "Universal Serial Bus controllers", right-click on the item"TI XDS100 Channel B". A properties dialog is shown. In the tab "Advanced", check the option "Load VCP". After the setting, I unplug and re-plug USB cable, then "USB Serial Port (COM6)" appears in the Device Manager.
I don't know if your case is the same as mine. But you can give it a try.
Btw, I am using CCSv6.1.2.