When I install ccs v6.1.1 for Linux 12.04 LTS, error occur. I refer Linux Host Support CCSv6, Ubuntu 14.04 32bit and execute sudo apt-get update, sudo apt-get installed libgnomeui-0 libusb-1.0-0-dev.
I am going to use Spectrum Digiatal XDS220ISO emulator.
I try to upload log file directly through error sending window during installation, error also occurred.
my name is yung and e mail yungyu@kmou.ac.kr
Here is last part of install_logs
***************************************
03/24/2016 06:35:58(GMT) - processOtherFeatures - Setting state to feature registered
03/24/2016 06:35:58(GMT) - get_percentage - values 34062355 544028237 35
03/24/2016 06:35:58(GMT) - get_percentage - increase by 2.19139806341
03/24/2016 06:35:58(GMT) - processOtherFeatures - CCS_INFO: binary ti_emupack_setup_6.0.14.5_linux_i386.bin; ext = .bin
03/24/2016 06:35:58(GMT) - InstallBins - .bin: ti_emupack_setup_6.0.14.5_linux_i386.bin --mode unattended --ccs true --prefix "/opt/ti/ccsv6" --eclipseprefix "/opt/ti/ccsv6/eclipse" --enable-components c6000,arm,davinci,omap,c5500,xds100,xds560
03/24/2016 06:35:58(GMT) - InstallBins - cmd = "/opt/ti/ccsv6/eclipse/downloads/ti_emupack_setup_6.0.14.5_linux_i386.bin" --mode unattended --ccs true --prefix "/opt/ti/ccsv6" --eclipseprefix "/opt/ti/ccsv6/eclipse" --enable-components c6000,arm,davinci,omap,c5500,xds100,xds560
03/24/2016 06:35:58(GMT) - InstallBins - CCS_INFO: Installing com.ti.emulation.pack.linux
03/24/2016 06:35:58(GMT) - InstallBins - CCS_INFO: error message: Installer payload initialization failed. This is likely due to an incomplete or corrupt downloaded file.
03/24/2016 06:36:08(GMT) - InstallBins - CCS_INFO: Installing com.ti.emulation.pack.linux
03/24/2016 06:36:08(GMT) - InstallBins - CCS_INFO: error message: Installer payload initialization failed. This is likely due to an incomplete or corrupt downloaded file.
03/24/2016 06:36:18(GMT) - InstallBins - CCS_INFO: Installing com.ti.emulation.pack.linux
03/24/2016 06:36:18(GMT) - InstallBins - CCS_INFO: error message: Installer payload initialization failed. This is likely due to an incomplete or corrupt downloaded file.
03/24/2016 06:36:18(GMT) - processOtherFeatures - CCS_INFO: Finished installing binary ti_emupack_setup_6.0.14.5_linux_i386.bin
03/24/2016 06:36:18(GMT) - processOtherFeatures - new state: install failed
03/24/2016 06:36:18(GMT) - checkStatus - CCS_ERROR: Installer failed to install com.ti.emulation.pack.linux correctly.
Please submit these logs to TI for analysis using the next dialog.
You may also visit the TI E2E CCS Support forum for additional help.
The install logs are located in: /opt/ti/ccsv6/install_logs.
03/24/2016 06:36:18(GMT) - checkStatus - file does not exist /tmp/ccs_9ac6c9bc-d027-4822-76ae-72fe3c33c4ac/eclipse/ws/.metadata/.log
03/24/2016 06:36:18(GMT) - checkStatus - saving /opt/ti/ccsv6/install_logs_20160324153116
03/24/2016 06:36:18(GMT) - checkStatus - saving /opt/ti/ccsv6/install_logs_20160322154508
03/24/2016 06:36:18(GMT) - checkStatus - saving /opt/ti/ccsv6/install_logs
03/24/2016 06:36:18(GMT) - checkStatus - saving /opt/ti/ccsv6/install_logs_20160324151159
03/24/2016 06:36:18(GMT) - checkStatus - CCS_ERROR: Code Composer Studio v6 installation failed.
root@ubuntu:/opt/ti/ccsv6/install_logs#
Please help me