This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DOCKING Station Error Message

Other Parts Discussed in Thread: TMS320F28027

I am Using TMS320F28027 docking station. I was working fine with that station. But after some days it gives a message like

 

Error connecting to the target:
Error 0x80000200/-1041
Fatal Error during: OCS,
Device driver: Problem with the Emulation Controller.
It is recommended to RESET EMULATOR.  This will disconnect each
target from the emulator.  The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.

 

what i want to do?

 

Please help me.

  • Hi Suresh,

    Please provide as much information as possible as requested in the forum readme: http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/3131.aspx

    The more details your provide, then better the chance we have to help you.

    Thanks,

    ki

  • Thank you soo.

     

    I am using Docking station USB-Emu [R3]. and the F2802xx (Piccolo-A)  Control CARD Release 1.0. i.e., TMS320F28027 control card.

     

    In CCSV4 version: 4.1.1.00014 can Build and debug that coding. i.e., LED blinking program. also my own coding. but I can't Debug the coding the last day. when I try to Debug it gives error message. The error message is

     

    Error connecting to the target:
    Error 0x80000200/-1041
    Fatal Error during: OCS,
    Device driver: Problem with the Emulation Controller.
    It is recommended to RESET EMULATOR.  This will disconnect each
    target from the emulator.  The targets should then be power cycled
    or hard reset followed by an emureset and reconnect to each target.

     

    I don't know how to reset the emulator. what is the way to do this?

     

    Thanks in advance.