This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Installing in common

Other Parts Discussed in Thread: CCSTUDIO

It is done!

It lasts from 9 AM till now ( 2 PM)!

And I get, trara:

The same as yesterday.

I've  found in the install_logs

ccs_setup_6.1.2.00015_install.log

First two lines

04/01/2016 07:29:08(GMT) - checkAV - CCS_INFO: av message child process exited abnormally
04/01/2016 07:29:12(GMT) - checkAVAgain - CCS_INFO: av message child process exited abnormally

To the End of File:

04/01/2016 09:16:50(GMT) - verifyInstall - Warnings: 0
04/01/2016 09:16:50(GMT) - verifyInstall - CCS_INFO: Code Composer Studio v6 Installation Complete.
04/01/2016 09:16:50(GMT) - verifyInstall - CCS_INFO: Code Composer Studio v6 has been successfully installed.

In another file : ccs_6.1.2.00015.log

[09:29:06] running C:\Users\admin\AppData\Local\Temp/ccs_d09c5807-1cdb-4b7f-6f55-02f934437754\tcl\bin\tclsh "C:/Users/admin/AppData/Local/Temp/ccs_d09c5807-1cdb-4b7f-6f55-02f934437754/installer_tcl/main_frontend/main.tcl" --installersrc "D:/Install" --installertmp "C:/Users/admin/AppData/Local/Temp/ccs_d09c5807-1cdb-4b7f-6f55-02f934437754"  --buildid 6.1.2.00015 --installer "D:/Install/ccs_setup_win32.exe" --bitness 64-bit --os windows
Executing C:\Users\admin\AppData\Local\Temp/ccs_d09c5807-1cdb-4b7f-6f55-02f934437754\tcl\bin\tclsh "C:/Users/admin/AppData/Local/Temp/ccs_d09c5807-1cdb-4b7f-6f55-02f934437754/installer_tcl/main_frontend/main.tcl" --installersrc "D:/Install" --installertmp "C:/Users/admin/AppData/Local/Temp/ccs_d09c5807-1cdb-4b7f-6f55-02f934437754"  --buildid 6.1.2.00015 --installer "D:/Install/ccs_setup_win32.exe"  --bitness 64-bit --os windows
Script exit code: 0

Script output:
 

Script stderr:
 

[11:40:44]

Why is there 2 hours  no feedback?

What does the message mean?

Observations::

The Java-Installation runs only with -Xmx 512M.

I saw in the initial intallation ( last about 3 hours) 4 processes UNPACK2000

Updates last terribly long.

No user response /feedback.

regards

Steffen

  • It doesn't work.
    ti_config_rtos doesn't know the Env-Variable:
    COM_TI_RTSC_TIRTOSCC32XX_REPOS

    I have ( only the most important):
    com.ti.ccstudio (6.1.1.201512011200) "CCS Product Branding"
    com.ti.ccstudio.base (6.1.0.01449) "CCS Base Components"
    org.eclipse.rtsc.xdctools.product_3.31.0.24 (3.31.0.24) "XDCtools Embedded Runtime Content"
    org.eclipse.rtsc.xdctools.product_3.31.1.33 (3.31.1.33) "XDCtools Embedded Runtime Content"
    org.eclipse.rtsc.xdctools.product_3.32.0.06 (3.32.0.06) "XDCtools Embedded Runtime Content"

    com.ti.rtsc.TIRTOSCC32XX.product_2.16.0.08 (2.16.0.08) "TI-RTOS for CC32XX Embedded Runtime Content" [Starting]
    com.ti.rtsc.TIRTOSCC32XX.product.ui (2.16.0.08) "TI-RTOS for CC32XX IDE Tooling" [Starting]
    com.ti.rtsc.TIRTOSCC32XX.productPlugin (2.16.0.08) "TI-RTOS for CC32XX Plugin" [Resolved]

    Please help! I don't know anymore what to do.
  • Steffen Netz said:
    It doesn't work.

    Sorry about the delayed reply, this thread seems to have fallen through the cracks.

    Can you please elaborate on what doesn't work? It seems that the CCS installation did complete successfully, even though it took a long time. 

    Are you now having trouble building projects? Please provide as much detail as possible so we can best try to assist you.