Other Parts Discussed in Thread: TMS320C6748, CCSTUDIO
I checked out the other posts that reported a similar issue. I am running Windows Vista 32-bit SP1 and I've made sure the UAC settings are Off. Also, I was running Symantec antivirus software but uninstalled it to try and correct this problem. I've also disabled Windows Defender and Firewall.
The problem occurs after installing the Code Composer v3.3 that was provided with the L138/TMS320C6748 EVM I just got. After you start the program from the desktop shortcut, it reaches the spash screen and hangs.
I previously had the CCS v4.1 evaluation software installed on the same computer and it ran fine. I uninstalled it before installing the v3.3 that came with the dev kit.
Does anyone have an idea about what else could be causing the problem?
Thanks!