Other Parts Discussed in Thread: CC1310
The following is the error message that I am getting. We are using the xds100V3 to debug our cc1310 MCU. I am using Windows 10, CCS v6, using a bread board to temporarily build our circuit, and the following image is the circuit design.
Error connecting to the target:
(Error -233 @ 0x0)
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
(Emulation package 6.0.83.1)
Could you help me figure what's going on with our debugging process?