Hi there,
I have messed up the default "Debug" build configuration, can I restore the “Debug” build configuration to its default state?
I tried go to Build Configurations -> Manage, Create a new configuration use copy settings from default configurations(choose any of default, debug or release):
After I click OK in the above picture, the "debugbackup" build configuration is truly created:
However, the new configuration will disappear after I click OK in the above picture...
If I choose create a new configuration use existing settings, it will not disappear... But I want to restore the default "Debug" build configuration, so I cannot create a new configuration from the existing "Debug" configuration...
Can this be fixed, or is there another way to restore the default "debug" build configuration?
Thanks!