Hi. I use a Mac and am trying to program a beagleboard (incl. JTAG XDS100 V2) - as far as I have read (processors.wiki.ti.com/.../VMware_with_CCS) this setup does not work well. I cannot seem to get it to work at all :o(
My setup:
Mac Pro 13" Retina i7 / 16 GB RAM / 256 SSD / VMWare Fusion 8.1.0 / OS X 10.11.4 / Windows 10 / CSS 6.1.2.00015
does anybody know of a way to make this work? I don't mind switching to Parallels if that helps, or using an older version of Windows (7, for example) or can I make some changes to the setup to get it working? Everything was working perfectly with the MSP430.
Thank you for any help given
Ursus