When I startup CCSv4.1.1.00014 it displays a message that says software updates are available. I download the softward and attempt to install it, at which point it displays the following message:
|
Duplicate Conflicts Detected conflicts: |
So because of its stern warnings, I cancel out of the update. Question: What is this weird behavior? What should I do about the update? So far, whenever I startup the program, it keeps telling me an update is available and asking me if I want to install it -- at which point I cancel the update.