Hi;
I am trying to add files from the "sprc832" software package into proj_lab04 in order to set up two nested interrupts inside the main ISR
(basically, I have two different motor control implementations written in an ISR- developed in different projects- each. I want one of the nested ISR's to run depending on conditions set in the background loop. I believe nesting the two ISRs will be much easier? am I current?)
The files from the sprc832 package are located in root directory C:\tidcs\c8\DSP2802x
When adding the files, I copied them directly into the project folder in the workspace, and added the #include files;
DSP2802x_Device.h and DSP2802x_Examples.h in the proj_lab04.c file
However, I keep getting the following error:
**** Build of configuration Flash for project proj_lab04 ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: C:/ti/motorware/motorware_1_01_00_16/sw/solutions/instaspin_foc/src/proj_lab04.c'
'Invoking: C2000 Compiler'
"C:/ti/ccsv6/tools/compiler/ti-cgt-c2000_6.4.6/bin/cl2000" -v28 -ml -mt -O2 --include_path="C:/tidcs/c28/DSP2802x/v126/DSP2802x_common/include" --include_path="C:/tidcs/c28/DSP2802x/v126/DSP2802x_common/source" --include_path="C:/ti/motorware/motorware_1_01_00_16/sw/modules/hal/boards/boostxldrv8301_revB/f28x/f2802x/src/" --include_path="C:/tidcs/c28/DSP2802x/v126/DSP2802x_common/cmd" --include_path="C:/tidcs/c28/DSP2802x/v126/DSP2802x_headers/include" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-c2000_6.4.6/include" --include_path="C:/ti/motorware/motorware_1_01_00_16/sw/solutions/instaspin_foc/boards/boostxldrv8301_revB/f28x/f2802xF/src" --include_path="C:/ti/motorware/motorware_1_01_00_16" -g --define=FLASH --define=FAST_ROM_V1p7 --define=F2802xF --diag_warning=225 --display_error_number --asm_listing --preproc_with_compile --preproc_dependency="proj_lab04.pp" "C:/ti/motorware/motorware_1_01_00_16/sw/solutions/instaspin_foc/src/proj_lab04.c"
"C:/ti/motorware/motorware_1_01_00_16/sw/solutions/instaspin_foc/src/proj_lab04.c", line 110: error #148: declaration is incompatible with "Uint16 RamfuncsLoadStart" (declared at line 88 of "C:\tidcs\c28\DSP2802x\v126\DSP2802x_common\include\DSP2802x_GlobalPrototypes.h")
"C:/ti/motorware/motorware_1_01_00_16/sw/solutions/instaspin_foc/src/proj_lab04.c", line 110: error #148: declaration is incompatible with "Uint16 RamfuncsLoadEnd" (declared at line 89 of "C:\tidcs\c28\DSP2802x\v126\DSP2802x_common\include\DSP2802x_GlobalPrototypes.h")
"C:/ti/motorware/motorware_1_01_00_16/sw/solutions/instaspin_foc/src/proj_lab04.c", line 110: error #148: declaration is incompatible with "Uint16 RamfuncsRunStart" (declared at line 90 of "C:\tidcs\c28\DSP2802x\v126\DSP2802x_common\include\DSP2802x_GlobalPrototypes.h")
3 errors detected in the compilation of "C:/ti/motorware/motorware_1_01_00_16/sw/solutions/instaspin_foc/src/proj_lab04.c".
>> Compilation failure
gmake: *** [proj_lab04.obj] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
The description of the problem states the following:
"#148 Declaration is incompatible with "Uint16 RamfuncsLoadEnd"
"#148 Declaration is incompatible with "Uint16 RamfuncsLoadStart"
"#148 Declaration is incompatible with "Uint16 RamfuncsRunStart"
Why am I getting this error, and How do I fix it?
{It must be pointed out;
for some reason, in my DSP2802x_Device.h file, the target hardware is set to be;
#define DSP28_28027PT TARGET
I am indeed using the f28027f Launchpad, so I am not sure why there is some variance in the definition, perhaps this is the problem?}
Also, which files am I actually supposed to modify in order set up the ISR's and then to link the PIEIER to the conditions set in the background loop in proj_lab04.c?
I am a little confused on this point, because the base project has a main interrupt without including the DSP2802x files, so perhaps there could be a way of achieving my goal without using these files
Thank you