I am using Docking station USB-Emu [R3]. and the F2802xx (Piccolo-A) Control CARD Release 1.0. i.e., TMS320F28027 control card.
In CCSV4 version: 4.1.1.00014 can Build and debug that coding. i.e., LED blinking program. also my own coding. but I can't Debug the coding the last day. when I try to Debug it gives error message. The error message is
Error connecting to the target:
Error 0x80000200/-1041
Fatal
Error during: OCS,
Device driver: Problem with the Emulation
Controller.
It is recommended to RESET EMULATOR. This will
disconnect each
target from the emulator. The targets should then
be power cycled
or hard reset followed by an emureset and reconnect
to each target.
I don't know how to reset the emulator. what is the way to do this?
Thanks in advance.