Hi.
i have started use CCS 4.1.2. it generates TI-TXT and INTEL-HEX files. But i want to *.cof or *.elf file.
Thanks...
http://focus.ti.com/lit/ug/slau157m/slau157m.pdf
2.1.5 How to Generate Binary-Format Files (TI-TXT and INTEL-HEX)
The CCS installation includes the hex430.exe conversion tool. It can be configured to generate output
objects in TI-TXT format for use with the MSP-GANG430 and MSP-PRGS430 programmers, as well as
INTEL-HEX format files for TI factory device programming. The tool can be used either standalone in a
command line (located in <Installation Root>\tools\compiler\msp430\bin) or directly within CCS. In the
latter case, a post-build step can be configured to generate the file automatically after every build by
selecting predefined formats such as TI-TXT and INTEL-HEX in the "Apply Predefined Step" menu
(Project → Properties → C/C++ Build → Build Steps → Post-Build Step). The generated file is stored in
the <Workspace>\<Project>\Debug\ directory.