Other Parts Discussed in Thread: CC1310
Hello,
I have a TI CC1310 development kit which consists of a SmartRF06 board and a CC1310 daughter board. I am running CCS 6.1.3. After installing the IDE I plugged in my development kit. The drivers seem to have installed correctly (the Windows Device Manager shows TI XDS100v3 Channel A and Channel B). After downloading a simple sample project and rebuilding it, I attempted to flash the program to my dev kit. I got the following error dialog:
There are a couple of issues:
- I checked the project debugger settings and there is only an option for XDS110v3 debugging. The Windows Device Manager and the dev kit documentation indicate that the board uses XDS100v3 emulation.
- As reported in other threads I tried swapping USB cables. I suspect this is not the issue as I am using the ones that came with the kit as well as another known good cable.
I am at the end of my rope trying to figure out what's wrong. Using the 'xdsdfu' utility shows 0 USB devices on the bus. I am plugged in directly to my PC (which is directly plugged in to a wall socket so that I can rule out laptop issues). I am running Windows 7 if that is of any information.
Has anyone encountered this issue before?
Many thanks!