To All,
Item 1:
I am using CCS as developemnt environment. Attached zip file contains the gel files and CMD file that we are using with our project to run from internal ram. I am using Development kit DK-LM3S9B96. This developemnt kit has 8 MByte of external RAM. I would like to create a test application that will get loaded into 8 Mbyte of external ram and run from external RAM. I also like to use the IDE debugger to debug the application that is running from external RAM. Any help you can provide will be very helpful.
Item 2.
I wanted to use the real time clock. Dose any one has an example code of to initialize and start real time clock using function call available in ROM library or drivver library?
Thanks.