CCS Champs,
I installed the CCS6.1.3 for 32 bit Sitara ARM processors and selected installation of the TI ARM compiler in the installer. However, after I download the package instead of TI ARM compiler 5.2.x compiler version, I see the TI ARM compiler version as ti-cgt-arm_15.12.1.LTS which appearss to be the MCU compiler.
Can you confirm that the TI ARM compiler for M3 and M4 has moved to the new version numbering or is this an issue where it is installing the MCU version of the compiler instead of the TI ARM 5.2.x version of the compiler.
Appreciate your support with this issue.
Regards,
Rahul