This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv6 internal webbrowser / resource explorer not showing (Ubuntu 16.04 amd64 / Arch Linux x86_64)

Hi,

I've installed CCSv6 on Ubuntu 16.04. The installation seems to be fine, but the resource explorer (I think this is a problem of the internal webbrowser) shows no content. I can switch between the examples on the left, but I can't open any. I've also tried to install CCSv6 on Arch Linux. After resolving the dependencies (expect libOrbit2) the installation seems to be fine as well. The resource explorer was working also, but since some days there's the exact same problem. Can somebody help me?

Thanks a lot!