This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000: Is "once in a while slow build issue" going to be fixed in CCSv6.3?

Guru 20075 points

Hello,

Has the slow build issue been fixed? I am using the C2000 compiler.

Stephen

  • Stephen,

    Is this the same issue as reported in the thread below?
    e2e.ti.com/.../1344626

    The short answer is no. Unfortunately without a consistent way to reproduce this our action is very limited. We can try to keep on the lookout for similar scenarios - are you experiencing this with CCSv6.1.3?

    Regards,
    Rafael
  • Hello Rafael,

    "Is this the same issue as reported in the thread below?"

    I think it happens when I create a new workspace and after I change to a different compiler.

    "are you experiencing this with CCSv6.1.3?"
    I haven't used CCSv6.1.3 long enough. I will report it if it does happen

    Stephen