This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Path Variable/Build Variable Issue with New Project CCS 6.1.3

Hey all,


I'm running into an issue with a new project I'm working on in CCS.  I started off with a template project I imported.  For some reason the path variables defaulted to the C:/Users director on my PC which is not what I'm looking for.  I updated the path variables and build variables to be correct, but that hasn't fixed the issue.  I looked under advanced features and the compiler says it can't find the files even though I've used the exact same path/build variables on another project. 

Any ideas?