This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Re:Stuck wid code for FSK(v.21) modem

Hi all!

I m new to CCS. I am trying to implement FSK(v.21) modem on C5510DSK board a/c to d steps given in d tutorial at d following links:

 

I am giving my code for d part upto filtering here:
#include "tonecfg.h"
#include "dsk5510.h"
#include "dsk5510_aic23.h"
#include<stdio.h>
#include<math.h>
/* Codec configuration settings */
DSK5510_AIC23_Config config = {
    0x0017, // 0 DSK5510_AIC23_LEFTINVOL  Left line input channel volume
    0x0017, // 1 DSK5510_AIC23_RIGHTINVOL Right line input channel volume
    0x00FF, // 2 DSK5510_AIC23_LEFTHPVOL  Left channel headphone volume
    0x00FF, // 3 DSK5510_AIC23_RIGHTHPVOL Right channel headphone volume
    0x0011, // 4 DSK5510_AIC23_ANAPATH    Analog audio path control
    0x0000, // 5 DSK5510_AIC23_DIGPATH    Digital audio path control
    0x0000, // 6 DSK5510_AIC23_POWERDOWN  Power down control
    0x0043, // 7 DSK5510_AIC23_DIGIF      Digital audio Int16erface format
    0x0081, // 8 DSK5510_AIC23_SAMPLERATE Sample rate control
    0x0001  // 9 DSK5510_AIC23_DIGACT     Digital Int16erface activation
};
#define FIRLEN 19 
float coefs[FIRLEN] = {-0.008370237662365, 0.003523724616947,  0.01237363596323,  0.02713952454333, 0.04697784958127,  0.06994028726489,  0.09309959888495,   0.1130209563111,  0.1265124921103,    0.131279039604,   0.1265124921103,   0.1130209563111,   0.09309959888495,  0.06994028726489,  0.04697784958127,  0.02713952454333,    0.01237363596323, 0.003523724616947,-0.008370237662365};
//Int16 inputs[30] = {1.13128697433765 ,1.10984462553037 ,1.38344070298819 ,0.626150903279837 ,0.274450597351357 ,0.580994546781292 ,0.237492756839462 ,0.679663383970494 ,0.322571475796019 ,1.21779302841047 ,0.570692318798823 ,1.16763875860796 ,0.653554635345044 ,0.714598072144237 ,0.726021551753316 ,0.905479767550582 ,0.00435839319756108 ,0.479972769744528 ,0.113617074520466 ,1.09094320060140 ,1.12589149609019 ,0.521013993015299 ,0.763457292330922 ,0.108789020498579 ,0.920646227924225 ,1.15623623159461 ,0.0791557324943119 ,1.09534727278226 ,0.148991578063601 ,0.6170647215283747}; 
extern void circbuff();      // defined in asmfunctions.asm
float *inPtr; //poInt16er to input sample
float *outPtr; //poInt16er to output
float *coeff; //poInt16er to the coefficients
//Int16 leftsample, rightsample;
//Int16 input=0;
float output=0;
Int16 sample1;
Int16 j,i; 
float mixerReal[120],mixerImg[120],mixer[120];
float mixerReal_param , mixerImg_param;
void filter_input(float*,float*,Int16);
void main()
{
    DSK5510_AIC23_CodecHandle hCodec;
    /* Initialize the board support library, must be called first */
    DSK5510_init();
    /* Start the codec */
    hCodec = DSK5510_AIC23_openCodec(0, &config);
DSK5510_AIC23_setFreq(hCodec, DSK5510_AIC23_FREQ_16KHZ);
   coeff = &coefs[0]; //coefs is coefficient of impulse response defined in fdacoefs_Int16.h
   inPtr = &mixer[0]; //inPtr is a globally declared poInt16er to a Int16 
   //inPtr = &mixerReal[0];
   outPtr = &output;
   
for ( j = 0; j < 120; j++ ) 
{
filter_input(&mixerReal_param,&mixerImg_param,j);
mixerReal[j]=mixerReal_param;
mixerImg[j]=mixerImg_param;
mixer[j]=mixerReal_param + mixerImg_param;
   
 
   
   
for(i=0;;i++)
{
for(sample1=0;sample1<120;sample1++)
{
 //while (!DSK5510_AIC23_read16(hCodec, mixer[sample1]));
 //while (!DSK5510_AIC23_read16(hCodec, mixer[sample1]));
      circbuff();
      
      
      
      
      
}      
      while (!DSK5510_AIC23_write16(hCodec, output));
      while (!DSK5510_AIC23_write16(hCodec, output));
}
   
    DSK5510_AIC23_closeCodec(hCodec);
}
void filter_input(float*mixerReal_dummy,float*mixerImg_dummy,Int16 j_dummy)
{
    float bitperiod = (1.0 / 300.0);
    float fs = 9000, f1 = 1650, f0 = 1850, fc = 1750;
    float temp  = 0.0;
    Int16 ii,jj,k=0;
    
    float input[4]={1.0,0.0,1.0,0.0};
    float modwave[120];
    float Cos[ 4 ], Sin [ 4 ];
    
    Int16 len = 0;
    float sample[30];
    for ( temp = (1/(fs+0.0)); temp <= bitperiod; temp += (1/(fs+0.0)) )
    {
         sample[len++] = ii;
    }
   
   ////////////////////////////////////////////////////////////////////////////////////
   ////////////////***   Modulation   ***//////////////////////////////////////////////
   ////////////////////////////////////////////////////////////////////////////////////
    
    //Int16 modwave[len * 4];
   // Int16 j=0, jj;
    for( ii = 0; ii < 4; ii++ ) {
         if(input[ii]) {
                for( jj = 0; jj < len; jj++ ) {
                     modwave[k++] = sin ( 2.0 * 3.1416 * (f1 + 0.0) * sample[jj] );
                     //prInt16f("%f ",modwave[j-1]);    
                } 
         } else { 
                for( jj = 0; jj < len; jj++ ) {
                     modwave[k++] = sin ( 2.0 * 3.1416 * (f0 + 0.0) * sample[jj] );
                     //prInt16f("%f ",modwave[j-1]);    
                }
         }
    }
           
   ////////////////////////////////////////////////////////////////////////////////////
   ////////////////***   Mixxing      ***//////////////////////////////////////////////
   ////////////////////////////////////////////////////////////////////////////////////
         
   //Int16 Cos[ 4 ], Sin [ 4 ];
      
   for ( jj = 0; jj < len; jj++ ) {
       Cos[jj] = cos( 2.0 * 3.1416 * (fc+0.0) * sample[jj] );
       Sin[jj] = sin( 2.0 * 3.1416 * (fc+0.0) * sample[jj] );
   }
      
  // Int16 mixerReal_dummy[len * 4], mixerImg_dummy[len * 4];
   
      *mixerReal_dummy = modwave[j_dummy] * Cos[j_dummy%len];
      *mixerImg_dummy = modwave[j_dummy] * Sin[j_dummy%len];
   
  // return (*mixerReal_dummy,*mixerImg_dummy);
   
}    
//ASM code for filtering:
      .ARMS_off                     ;enable assembler for ARMS=0
      .CPL_on                       ;enable assembler for CPL=1
      .mmregs                       ;enable mem mapped register names
.global _circbuff
.global _inPtr ;global declarations
.global _outPtr
.global _coeff
; This is a skeleton project for initializing circular buffer
.data ;data section
;section where all the data is stored 
FIR_len .set 12 ;length of the impulse response determines buffer space ex: 4 length filter
.align 16
firbuff .space 16*FIR_len ; allocating buffer space
oldindex .word  0 ; Allocate storage to save oldindex (defines where next sample 
;has to be put in buffer)
.text ;this section contains the code 
_circbuff ;function definition
   MOV #FIR_len, BK03             ; Circular buffer size is 3 words
   BSET AR1LC               ; AR1 is configured to be modified circularly
   ;AMOV #010000h, XAR1      ; Circular buffer is in main data page 01
   MOV #firbuff, BSA01        ; Circular buffer start address is 010A02h
   ;AMOV #_inPtr, XAR1       ; XAR1 == AR1H:AR1   &&   ARnH:(BSAxx + ARn) 
   MOV *(#oldindex), AR1          ; Index (in AR1) is 0000h
   MOV dbl(*(#_inPtr)), XAR6
   MOV dbl(*(#_outPtr)), XAR7
   MOV dbl(*(#_coeff)), XAR2
   MOV *AR6, *AR1+
   MOV AR1, *(#oldindex) 
 
; initialization done here 
; processing starts below 
 
   MOV #0h, AC1 
   BCLR AR2LC        ; XAR2 is linear buffer
   RPT #11            
   MACM *AR1+, *AR2+, AC1
   MOV HI(AC1), *AR7
; section 1: loading address
;ex:-
; MOV dbl(*(#_inPtr)), XAR6 ; XAR6 contains address to input
; check in help file and web link given in tutorial for syntax
; section 2: here set circular addressing for any ARn using the help file
; once set store the index of oldest state in this register
;ex:-
; MOV *AR6+, *ARn ; Receive input and store it in the location pointed by
; the circular buffer register
; Save the index of the oldest sample back into the location oldindex
RET
-------------XX---------------------
Can anybody sort out my problem?
Thanks in advance.
Kirti
 

 

  • If the compiler tools are giving you some diagnostic messages when you build, I might be able to help.  I need to see those messages.  If anything else is going wrong, I don't see how a compiler expert like me can help.

    Thanks and regards,

    -George