Other Parts Discussed in Thread: AM3358
Gentlemen,
Windows 7 64-bit PC
AM3358 on the AM335x Starter Kit
CCS Version: 6.1.2.00015 (for Sitara processors)
Processor SDK RTOS AM335x v2.00.02.11 with SYS/BIOS 6.45.01.29
XDCtools 3.32.00.06
PRU Support Package v4.0.2
I would like to call to the attention of the CCS engineers a conflict I recently encountered regarding the *.H file contents of the C:\ti\ccsv6\ccs_base\pru\include directory.
I encountered the conflict after a previously compiling PRU example started having errors compiling after I had switched the target device from "Beaglebone Black" to "SK_AM3358".
Investigating this, I found that the change caused
C:\ti\ccsv6\ccs_base\pru\include
to be (silently) inserted at the top of the Include directory list.
Investigating further, I found that some files in that directory are expressed only once (e.g. pru_cfg.h and pru_intc.h) whereas the contents of these files appear to change widely depending on which Sitara family is used. Specific example, the pru_cfg.h file differences between the AM335x vs AM437x are considerable (there appears to be a whole set of registers that exist for the AM437x and not for the AM335x). Furthermore, there a few minor bit-field width differences, for example the HIEISR.HINT_EN_SET_IDX field width in the INTC group of registers should be 4 bits for the AM335x, but the <ccs6>\ccs_base\pru\include\pru_intc.h files has this field width as 10 bits.
It would appear that the PRU Support Package v4.0.2 corrects these problems, but has no instructions about where to install it, and it would seem that once this is installed that it should somehow supplant the *.H files in the C:\ti\ccsv6\ccs_base\pru\include directory, especially since CCS6 is silently (probably correctly) ensuring that include directory is in a PRU project. Furthermore, the PRU Support Package v4.0.2 also includes different copies of 8 PRU .H files in separate directories for each Sitara processor family (am335x, am437x, am571x, etc.).
In case these things were not already on the list for resolution for the next CCS update, I thought I would bring them to your attention.
Kind regards,
Vic