Other Parts Discussed in Thread: CCSTUDIO
Hi,
I installed ccs_setup_5.5.0.00077.bin under centos 7.2. After running the full CCS installation, the output messages from the installer indicate that it completed successfully but the CCS launcher icon was not placed on my desktop. I tried starting the ccstudio executable from a terminal window and get the following error messages:
libgcc_s.so.1: cannot open shared object file: No such file or directory
Ccstudio: The Ccstudio executable launcher was unable to locate its companion shared library.
Does anyone have any ideas why the launcher icon is not on the desktop and/or how I can get the CCS program to run?
Suggestions would be greatly appreciated,
Jim Conway