Other Parts Discussed in Thread: CC3200
Hello All,
I was working on my project, using the CC3200 rev4.1, CCS 6.1.2.00015, SDK 1.2.0, that compiled (links/libraries setup) last week. This morning I access my project workspace and the build fails " implicit declarations" that link to files in the example/common folder and a linked file symbol in the project directory (i2c_if.c & gpio_if.c). The library is part of the build file path and resources that are linked, what I a missing?
And yes I'm new to CCS.
The functions in question are the report/ noterm and ic2_if_open!
Thanks,
Spiros