My intention is to run the audioenc application which is part of the Codec Engine on the dsp using CCS and app.out from Linux. I intend to extend the functionality of the audioenc application to implement my codec.
I placed the code snippet
Engine_open( .... );
printf("Hit enter to continue:");
getchar();
In the example application.
On the application side.
I ran ./app.out.
On the DSP side. I opened CCS V4.
Launched the config file.
Connected the DSP.
Loaded symbols (Target->Load Symbols->all.x64P).
Pressed F8.
Returned to the arm side and pressed the enter key.
What I see on the DSP side is that the control does not goto audioenc_copy which is the aim of my exercise.
Could someone help me out ??
I performed all these steps after referring to the link
http://processors.wiki.ti.com/index.php/Debugging_the_DSP_side_of_a_CE_application_using_CCS