When debugging my code and stopping in a function that comes from our own library (containing assembly modules), I get the info:
No source available for "function() at C:/Projects\myproject\myfile.out:{3} 0x130f8{4}"
There is no "locate sourcefile" button.
The library is built with "--symdebug:coff".
The assembly file contains the following statements:
.sym _function,32,2,0
.func
.global _function
.text
_function:
...function code...
.endfunc
What can be the problem?
What statements have to reside inside the assembly library function to be correctly located in the debugger?
CCS 6.1.3.00033
cgtools 15.12.2