Other Parts Discussed in Thread: CCSTUDIO
Hello there,
I tried installing CCS 6.1 today and I got an error message during installation pointing me to a log file which I have attached in this message below. I can start CCS 6.1 after this failed installation, but I keep getting strange error messages (can't list them all) when I open for the first time, and when I try to do certain actions like import a project. I am still poking around to see if I can compile and run a simple project. Let me know if you have any idea what could be the problem. My operating system is Windows 7, 64 bit, with 16GB of RAM. Ok, here is the error log I mentioned:
!SESSION 2016-05-12 14:05:13.353 -----------------------------------------------
eclipse.buildId=4.5.1.M20150904-0015
java.version=1.7.0_80
java.vendor=Oracle Corporation
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en_US
Framework arguments: -application com.ti.common.core.initialize -ccs.profileTag Installed Code Composer Studio 6.1.3.00033.
Command-line arguments: -os win32 -ws win32 -arch x86 -application com.ti.common.core.initialize -data C:/Users/Admin/AppData/Local/Temp/ccs_4c8254b3-52bd-4a0c-531d-ac7edf049623/workspace -ccs.profileTag Installed Code Composer Studio 6.1.3.00033.
!ENTRY com.ti.common.core 4 0 2016-05-12 14:05:21.438
!MESSAGE path=ccs_base/DebugServer
!ENTRY com.ti.common.core 4 0 2016-05-12 14:05:21.439
!MESSAGE debugServerDir=C:/ti/ccsv6/ccs_base/DebugServer
!ENTRY org.eclipse.core.jobs 4 2 2016-05-12 14:05:22.184
!MESSAGE An internal error occurred during: "CrashTrackerJob".
!STACK 0
java.lang.UnsatisfiedLinkError: C:\ti\ccsv6\ccs_base\DebugServer\bin\LibraryLoader.dll: Can't find dependent libraries
at java.lang.ClassLoader$NativeLibrary.load(Native Method)
at java.lang.ClassLoader.loadLibrary1(ClassLoader.java:1965)
at java.lang.ClassLoader.loadLibrary0(ClassLoader.java:1890)
at java.lang.ClassLoader.loadLibrary(ClassLoader.java:1851)
at java.lang.Runtime.load0(Runtime.java:795)
at java.lang.System.load(System.java:1062)
at com.ti.debug.engine.xpcom.Runtime.preXPCOMInit(Runtime.java:163)
at com.ti.debug.engine.xpcom.Runtime.startBare(Runtime.java:116)
at com.ti.debug.engine.xpcom.Runtime.createComponent(Runtime.java:170)
at com.ti.utility.filesystem.DirectoryService.<init>(DirectoryService.java:26)
at com.ti.utility.filesystem.DirectoryService.<init>(DirectoryService.java:9)
at com.ti.utility.filesystem.DirectoryService$SingletonHolder.<clinit>(DirectoryService.java:44)
at com.ti.utility.filesystem.DirectoryService.instance(DirectoryService.java:49)
at com.ti.ccstudio.debug.server.DebugServerPlugin$1.run(DebugServerPlugin.java:117)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:55)
!ENTRY org.eclipse.osgi 4 0 2016-05-12 14:05:24.373
!MESSAGE Application error
!STACK 1
java.lang.NoClassDefFoundError: Could not initialize class com.ti.utility.filesystem.DirectoryService$SingletonHolder
at com.ti.utility.filesystem.DirectoryService.instance(DirectoryService.java:49)
at com.ti.common.core.utils.ds.CoreUtilsProvider.getUserHomeDir(CoreUtilsProvider.java:40)
at com.ti.common.core.CoreUtils.getUserHomeDir(CoreUtils.java:135)
at com.ti.common.core.internal.ExternalReferenceParser.getUserExtRefDir(ExternalReferenceParser.java:176)
at com.ti.common.core.internal.ExternalReferenceParser.getExtRefDirectories(ExternalReferenceParser.java:158)
at com.ti.common.core.internal.ExternalReferenceParser.getReferenceFiles(ExternalReferenceParser.java:61)
at com.ti.common.core.internal.ExternalReferenceParser.getReferenceFiles(ExternalReferenceParser.java:147)
at org.eclipse.rtsc.xdctools.managedbuild.core.products.RTSCProductDiscoveryManager.getExtensionSiteDiscoveryPath(RTSCProductDiscoveryManager.java:457)
at org.eclipse.rtsc.project.core.extdiscovery.ExtensionSiteDiscoveryManager.getUserSearchPath(ExtensionSiteDiscoveryManager.java:122)
at org.eclipse.rtsc.project.core.extdiscovery.ProductManifestRegistry.<init>(ProductManifestRegistry.java:84)
at org.eclipse.rtsc.project.core.extdiscovery.ProductManifestRegistry.<clinit>(ProductManifestRegistry.java:73)
at org.eclipse.rtsc.project.core.extdiscovery.ExtensionSiteDiscoveryManager.collectExtensionSiteDirsToAdd(ExtensionSiteDiscoveryManager.java:749)
at org.eclipse.rtsc.project.core.extdiscovery.ExtensionSiteDiscoveryManager.createExtensionSites(ExtensionSiteDiscoveryManager.java:214)
at org.eclipse.rtsc.project.core.extdiscovery.ExtensionSiteDiscoveryManager.createAndAddExtensionSites(ExtensionSiteDiscoveryManager.java:169)
at org.eclipse.rtsc.project.core.extdiscovery.RTSCIDEInitializationParticipant.run(RTSCIDEInitializationParticipant.java:89)
at com.ti.common.core.internal.headless.Initialize.run(Initialize.java:45)
at com.ti.common.core.internal.headless.Initialize.start(Initialize.java:32)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:380)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:235)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:57)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:606)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:669)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:608)
at org.eclipse.equinox.launcher.Main.run(Main.java:1515)