This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to install Code Composer 6.1.2. Help

Hello, I have downloaded Code Composer 6.1.2 twice and it fails that the same place. Here is the log file:

05/13/2016 16:49:27(GMT) - extract - file c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/jre_root_1.7.0.60 doesn't exist
05/13/2016 16:49:37(GMT) - extract - file c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/jre_root_1.7.0.60 doesn't exist
05/13/2016 16:49:47(GMT) - checkStatus - CCS_ERROR: Installer failed to install jre correctly. The 2 most common reasons for failure are:
 1.  Anti-virus on your computer could have impeded the executable.
 2.  Download is corrupted.
Please submit these logs to TI for analysis using the next dialog.
You may also visit the TI E2E CCS Support forum for additional help.

Can anyone suggest a fix?

Thanks, Joe

05/13/2016 16:48:26(GMT) - checkAV - CCS_INFO: av message 
05/13/2016 16:48:27(GMT) - checkAVAgain - CCS_INFO: av message 
05/13/2016 16:48:37(GMT) - checkProgramFiles - CCS_INFO: checking c:\program files (x86)
05/13/2016 16:48:37(GMT) - checkProgramFiles - CCS_INFO: checking c:\program files (x86)
05/13/2016 16:48:37(GMT) - checkProgramFiles - CCS_INFO: checking c:\program files
05/13/2016 16:48:37(GMT) - Util::httpCopy - http::config now: -accept */* -proxyfilter http::ProxyRequired -proxyhost {} -proxyport {} -urlencoding utf-8 -useragent {Tcl http client package 2.5.2}
05/13/2016 16:48:37(GMT) - Util::httpCopy - Downloading c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/apps_6.1.2.json from http://software-dl.ti.com/ccs/non-esd/ccs_appcenter/apps_6.1.2.json
05/13/2016 16:48:49(GMT) - Util::httpCopy - Could not get file http://software-dl.ti.com/ccs/non-esd/ccs_appcenter/apps_6.1.2.json:couldn't open socket: invalid argument
05/13/2016 16:49:06(GMT) - writeDebugFile - 

Install Information:


05/13/2016 16:49:06(GMT) - writeDebugFile - Install Version:  6.1.2.00015
05/13/2016 16:49:06(GMT) - writeDebugFile - Install Source	: D:/cc_install/CCS6.1.2.00015_win32
05/13/2016 16:49:06(GMT) - writeDebugFile - Install Temp	: c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e
05/13/2016 16:49:06(GMT) - writeDebugFile - Install Type	: Offline
05/13/2016 16:49:06(GMT) - writeDebugFile - OS				: Windows NT
05/13/2016 16:49:06(GMT) - writeDebugFile - OS	Version		: 6.1
05/13/2016 16:49:06(GMT) - writeDebugFile - OS	Platform	: windows
05/13/2016 16:49:06(GMT) - writeDebugFile -  				: 64-bit
05/13/2016 16:49:06(GMT) - writeDebugFile - User ID		: $a_bjp
05/13/2016 16:49:06(GMT) - writeDebugFile - Timezone		: Pacific Daylight Time
05/13/2016 16:49:06(GMT) - writeDebugFile - IPAddress		: 192.168.16.131
05/13/2016 16:49:06(GMT) - writeDebugFile - Update/Rerun	: 0
05/13/2016 16:49:06(GMT) - writeDebugFile - Command line	: installersrc D:/cc_install/CCS6.1.2.00015_win32 installertmp c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e buildid 6.1.2.00015 installer D:/cc_install/CCS6.1.2.00015_win32/ccs_setup_6.1.2.00015.exe bitness 64-bit os windows

05/13/2016 16:49:06(GMT) - writeDebugFile - 
Product families selected: 
05/13/2016 16:49:07(GMT) - writeDebugFile - PF_STELLARIS
05/13/2016 16:49:07(GMT) - writeDebugFile - PF_SITARA
05/13/2016 16:49:07(GMT) - writeDebugFile - PF_OMAPL13
05/13/2016 16:49:07(GMT) - writeDebugFile - PF_C6000_SINGLE
05/13/2016 16:49:07(GMT) - writeDebugFile - PF_C6000_MULTI
05/13/2016 16:49:07(GMT) - writeDebugFile - 
Components to be installed: 
05/13/2016 16:49:07(GMT) - writeDebugFile - EMU_STELLARIS
05/13/2016 16:49:07(GMT) - writeDebugFile - TIVA_STELLARIS_DRIVERS
05/13/2016 16:49:07(GMT) - writeDebugFile - TIVA_TM4C
05/13/2016 16:49:07(GMT) - writeDebugFile - TIVA_TM4E
05/13/2016 16:49:07(GMT) - writeDebugFile - EMU_HERCULES
05/13/2016 16:49:07(GMT) - writeDebugFile - ARM_CGT_HELP
05/13/2016 16:49:07(GMT) - writeDebugFile - CGT_DEFAULTLIBS_TMS470
05/13/2016 16:49:07(GMT) - writeDebugFile - DMED
05/13/2016 16:49:07(GMT) - writeDebugFile - GCC_ARM_COMPILER
05/13/2016 16:49:07(GMT) - writeDebugFile - C6000_CGT_HELP
05/13/2016 16:49:07(GMT) - writeDebugFile - CGT_DEFAULTLIBS_C6000_V8P
05/13/2016 16:49:07(GMT) - writeDebugFile - DEV_SUPPORT_INTEGRA
05/13/2016 16:49:07(GMT) - writeDebugFile - CGT_DEFAULTLIBS_C6000
05/13/2016 16:49:07(GMT) - writeDebugFile - DEV_SUPPORT_C6000
05/13/2016 16:49:07(GMT) - writeDebugFile - KEYSTONE1
05/13/2016 16:49:07(GMT) - writeDebugFile - KEYSTONE2
05/13/2016 16:49:07(GMT) - writeDebugFile - DEV_SUPPORT_C6000MC
05/13/2016 16:49:07(GMT) - writeDebugFile - EMU_TI
05/13/2016 16:49:07(GMT) - writeDebugFile - JRE
05/13/2016 16:49:07(GMT) - writeDebugFile - P2APP
05/13/2016 16:49:07(GMT) - writeDebugFile - ECLIPSE
05/13/2016 16:49:07(GMT) - writeDebugFile - ECLIPSECORE
05/13/2016 16:49:07(GMT) - writeDebugFile - P2TOOLS
05/13/2016 16:49:07(GMT) - writeDebugFile - GMF
05/13/2016 16:49:07(GMT) - writeDebugFile - IDE_MAIN
05/13/2016 16:49:07(GMT) - writeDebugFile - IDE_WORKFLOW
05/13/2016 16:49:07(GMT) - writeDebugFile - DVT_COMMON
05/13/2016 16:49:07(GMT) - writeDebugFile - DVT_UIA
05/13/2016 16:49:07(GMT) - writeDebugFile - DVT_VIA_CCS
05/13/2016 16:49:07(GMT) - writeDebugFile - INSTALLER
05/13/2016 16:49:07(GMT) - writeDebugFile - IDE_CHROME
05/13/2016 16:49:07(GMT) - writeDebugFile - IDE_TOOLS_COMMON
05/13/2016 16:49:07(GMT) - writeDebugFile - IDE_GC
05/13/2016 16:49:07(GMT) - writeDebugFile - TARGET_CONTENT_CORE
05/13/2016 16:49:07(GMT) - writeDebugFile - IDE_ARM
05/13/2016 16:49:07(GMT) - writeDebugFile - DVT_TRACE
05/13/2016 16:49:07(GMT) - writeDebugFile - DS
05/13/2016 16:49:07(GMT) - writeDebugFile - DS_FLASH
05/13/2016 16:49:07(GMT) - writeDebugFile - MSVC80
05/13/2016 16:49:07(GMT) - writeDebugFile - MSVC2012
05/13/2016 16:49:07(GMT) - writeDebugFile - DEV_SUPPORT_SITARA
05/13/2016 16:49:07(GMT) - writeDebugFile - DEV_SUPPORT_SHARED
05/13/2016 16:49:07(GMT) - writeDebugFile - BBONE_FTDI_DRIVERS
05/13/2016 16:49:07(GMT) - writeDebugFile - IDE_C6000
05/13/2016 16:49:07(GMT) - writeDebugFile - IDE_C5500
05/13/2016 16:49:07(GMT) - writeDebugFile - 
Apps to be installed when CCS starts up: 
05/13/2016 16:49:07(GMT) - getprefix - installdir for ARM_CGT_HELP: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for C2000_CGT_HELP: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for C5500_CGT_HELP: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for C6000_CGT_HELP: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getinstalluninstallcmds - Did not find matching component in InstallIni CCS_DOC. Using Defaults.
05/13/2016 16:49:07(GMT) - getinstalluninstallcmds - Did not find matching component in InstallIni CCS_LAUNCHER. Using Defaults.
05/13/2016 16:49:07(GMT) - getinstalluninstallcmds - Did not find matching component in InstallIni CCS_UTILS. Using Defaults.
05/13/2016 16:49:07(GMT) - getprefix - installdir for DVT_COMMON: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for DVT_ENERGYTRACE: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for DVT_TRACE: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for DVT_UIA: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for DVT_VIA_CCS: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for ECLIPSE: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for EMU_SD: c:/ti/ccsv6/ccs_base
05/13/2016 16:49:07(GMT) - getprefix - installdir for GMF: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for IDE_ARM: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for IDE_C2000: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for IDE_C5500: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for IDE_C6000: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for IDE_CHROME: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for IDE_GC: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for IDE_MAIN: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for IDE_MSP430: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for IDE_TOOLS_COMMON: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for IDE_WORKFLOW: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for KEYSTONE1: c:/ti/ccsv6/ccs_base
05/13/2016 16:49:07(GMT) - getprefix - installdir for KEYSTONE2: c:/ti/ccsv6/ccs_base
05/13/2016 16:49:07(GMT) - getprefix - installdir for MSP430_CGT_HELP: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getinstalluninstallcmds - Did not find matching component in InstallIni MSVC_REDIST_2005. Using Defaults.
05/13/2016 16:49:07(GMT) - getprefix - installdir for MSVC_REDIST_2005: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getinstalluninstallcmds - Did not find matching component in InstallIni MSVC_REDIST_2012. Using Defaults.
05/13/2016 16:49:07(GMT) - getprefix - installdir for MSVC_REDIST_2012: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for P2APP: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getprefix - installdir for P2TOOLS: c:/ti/ccsv6/
05/13/2016 16:49:07(GMT) - getinstalluninstallcmds - Did not find matching component in InstallIni TARGETDB_DEF_PROPS. Using Defaults.
05/13/2016 16:49:07(GMT) - getprefix - installdir for TARGET_CONTENT_CORE: c:/ti/ccsv6/..
05/13/2016 16:49:07(GMT) - Util::getProperty - No c:/ti/ccsv6/eclipse/ccs.properties file found
05/13/2016 16:49:07(GMT) - Util::getProperty - No c:/ti/ccsv6/eclipse/ccs.properties file found
05/13/2016 16:49:07(GMT) - ProgressPane::Run - Starting install process in separate thread
05/13/2016 16:49:07(GMT) - ProgressPane::Run - call = RunInstall c:/ti/ccsv6/eclipse/ccs_config.xml 0 0 0 0 c:/ti/ccsv6/install_logs/ccs_setup_6.1.2.00015_install.log ::progressPane0 tid00001314
05/13/2016 16:49:07(GMT) - ProgressPane::Run - separate threads
05/13/2016 16:49:07(GMT) - ProgressPane::Run - thread = tid00001488
05/13/2016 16:49:07(GMT) - RunMain - Started with params pConfigFile=c:/ti/ccsv6/eclipse/ccs_config.xml pProfiling=0 pUpdate=0 logfile=c:/ti/ccsv6/install_logs/ccs_setup_6.1.2.00015_install.log progress=::threadedProgressUpdate0
05/13/2016 16:49:07(GMT) - RunMain - encoding = cp1252
05/13/2016 16:49:07(GMT) - readConfigFile - Start installing components:
05/13/2016 16:49:07(GMT) - readConfigFile - read config file c:/ti/ccsv6/eclipse/ccs_config.xml
05/13/2016 16:49:07(GMT) - readConfigFile - found c:/ti/ccsv6/eclipse/ccs_config.xml
05/13/2016 16:49:07(GMT) - readConfigFile - Parsing Root Elements
05/13/2016 16:49:07(GMT) - readConfigFile - Done Parsing
05/13/2016 16:49:07(GMT) - readConfigFile - CCSDIR=c:/ti/ccsv6
05/13/2016 16:49:07(GMT) - readConfigFile - EclipseDir=c:/ti/ccsv6/eclipse
05/13/2016 16:49:07(GMT) - readConfigFile - InstallDir=c:/ti
05/13/2016 16:49:07(GMT) - readConfigFile - TempDir=c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e
05/13/2016 16:49:07(GMT) - readConfigFile - platform=windows
05/13/2016 16:49:07(GMT) - readConfigFile - LocalBaseRepository=D:/cc_install/CCS6.1.2.00015_win32/baserepo
05/13/2016 16:49:07(GMT) - readConfigFile - baserepourl=D:/cc_install/CCS6.1.2.00015_win32/baserepo
05/13/2016 16:49:07(GMT) - readConfigFile - featureurl=D:/cc_install/CCS6.1.2.00015_win32/featurerepo
05/13/2016 16:49:07(GMT) - readConfigFile - LocalRepository_Exists=1
05/13/2016 16:49:07(GMT) - readConfigFile - componentinstaller=false
05/13/2016 16:49:07(GMT) - readConfigFile - eclipseexe=eclipsec.exe
05/13/2016 16:49:07(GMT) - readConfigFile - in install components
05/13/2016 16:49:07(GMT) - readUserProfile - userprofile = C:\Users\$a_bjp
05/13/2016 16:49:07(GMT) - downloadIfRequired - deleted c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/jre_root_1.7.0.60
05/13/2016 16:49:07(GMT) - downloadIfRequired - File c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/jre_root_1.7.0.60 already exists. Not attempting to download
05/13/2016 16:49:07(GMT) - extract - file c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/jre_root_1.7.0.60 doesn't exist
05/13/2016 16:49:17(GMT) - extract - file c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/jre_root_1.7.0.60 doesn't exist
05/13/2016 16:49:27(GMT) - downloadIfRequired - deleted c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/jre_root_1.7.0.60
05/13/2016 16:49:27(GMT) - downloadIfRequired - File c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/jre_root_1.7.0.60 already exists. Not attempting to download
05/13/2016 16:49:27(GMT) - extract - file c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/jre_root_1.7.0.60 doesn't exist
05/13/2016 16:49:37(GMT) - extract - file c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/jre_root_1.7.0.60 doesn't exist
05/13/2016 16:49:47(GMT) - checkStatus - CCS_ERROR: Installer failed to install jre correctly. The 2 most common reasons for failure are:
	1.  Anti-virus on your computer could have impeded the executable.
	2.  Download is corrupted.
Please submit these logs to TI for analysis using the next dialog.
You may also visit the TI E2E CCS Support forum for additional help.

The install logs are located in: c:/ti/ccsv6/install_logs.
05/13/2016 16:49:47(GMT) - checkStatus - file does not exist c:/temp/ccs_b67e4e56-4362-4024-56e5-670ce167814e/eclipse/ws/.metadata/.log
05/13/2016 16:49:47(GMT) - checkStatus - saving c:/ti/ccsv6/install_logs
05/13/2016 16:49:47(GMT) - checkStatus - saving c:/ti/ccsv6/install_logs_20160513094906
05/13/2016 16:49:47(GMT) - checkStatus - CCS_ERROR: Code Composer Studio v6 installation failed.

  • Joe,

    From the log I suspect a few things:
    - Line 145 indicates you have a special character in your username. Historically this has been a source of problems.
    - Lines 146 through 153 indicate that the component named jre_root_1.7.0.60 was correctly extracted and copied to the temporary directory but it was immediately deleted. This is an indicative of external factors influencing the installation process - by that I mean an antivirus, anti-spyware or a corporate policy that prevents certain files or access types to the temporary area of your system.

    In this case I can only recommend you to temporarily disable the antivirus software running in your system or perhaps check for help from your IT department and see if there is any policy that prevents installation of these components.

    From the logs it seems you properly extracted the CCS off-line installer to D:\cc_install, is that correct? The reason of my question is that sometimes developers try to run the installer directly from the .zip file, which consequently causes problems.

    Hope this helps,
    Rafael