This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with Debugging TMDSHVMTRPFCKIT



Hi,

When I attempt to debug the HVACI_Sensored project with the "Enable silicon real-time mode" and/or "Enable polite real-time mode" options selected, I receive the following error message in the console: "C28xx: Error connecting to the target: Error 0x80000200/-1142 Fatal Error during: OCS,  Processor blocked debug accesses."

The only way that I have been able to get around it is by the following method: start debugging with no real-time options selected.  While debugging, select the option to "Enable polite real-time mode", apply, and then click debug to restart debugging.  Then, go back into the debug options again and select "Enable polite real-time mode," apply, and then click debug to restart debugging.  Then I have to stop the debugger, and then start it again and it works, but with the following error message in the console:

"C28xx: Trouble Writing Register ST1: Error 0x00000004/-2012 Error during: Register,  Cannot perform operation while CPU is running free. 
C28xx: GEL: Error while executing OnTargetConnect(): target access failed.
C28xx: Failed Software Reset: Error 0x00000020/-1138 Error during: Execution,  Processor aborted debug context. 
C28xx: Failed Software Reset: Error 0x00000020/-1138 Error during: Execution,  Processor aborted debug context."

Can anyone help me out?

Thanks,

John