This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

enum problem in Cla1ToCpuMsgRAM section

Genius 5910 points

I have the following problem:

I have a struct that communicate with the CLA in that struct there is  a enum. at the beginning the emun is cleared. but oddly enough there is a really big value in the enum  like 0x89E0000. If  I change state it change to 0x89E0001, etc. But the enum doesn't work correctly.

If I manually clear the whole value everything works fine.

I use: C2000 TI 6.4.10
So how do I solve this?

Thanks

 

 

  • I'm not sure I understand. I think you are saying a memory location changes values for no apparent reason. That sounds like a hardware issue that we compiler experts cannot help with.

    Thanks and regards,

    -George

  • typedef enum
    {
    Done=0,
    Init,
    Start,
    Rampup,
    Rampdown,
    } MOSPROF_State;

    State=Done (result in 0x89E0000)
    State=Init (0x89E0001)
    If I move the state variable around in the struct that communicate with the CLA the problem moves with it. so I don't think it is a hardware issue.
  • evs said:
    State=Done (result in 0x89E0000)
    State=Init (0x89E0001)

    Exactly how do you see these results?   -George

  • On C2000, that enum will be the same size as "int," which is 16 bits. The adjacent 16 bits with contents 0x89E0 are not part of the variable "State."
  • In the expression window with CCS debuger.
  • That can be true. But the state machine isn't working. If it happens to be 0 or I change it in CCS debuger to the state done. The code works correctly. The variable description in CCS debug expression window is: enum unknown.

    So somehow in CpuToCla1MsgRAM or in CLA a enum is defined as 32 bit and in the main code as 16 bit. That should explain the problem.

    edit:

     if I do a sizeof the MOSPROF_State enum i got 2

    Sizeof enum in CLA memory is also 2

    Sizeof enum(normal memory)  the size is 1.

    So that is the problem.

    Disassembly:

    166         Servo_profile_init.state=Done;
    3eac6e:   2B02        MOV          @0x2, #0  

    That is a 16bit move and not a 32bit. This state is copied to the CLA and the uninitialized high word is then part of the result.
     

  • You are correct about the sizes of enum types.  On C28x, they are 16-bits.  On CLA, they are 32-bits.  It is similar to the problem with the size of pointers.  The pointer size problem, and a solution, is discussed in this wiki article.  You need to adopt a similar solution for any enum type shared between C28x and CLA.

    Thanks and regards,

    -George

  • I think that pointer alignment and 32 vs 16 bit  enums cast are a complete a difference  thing.  You know that also.

     

  • But the solution is the same: establish a union between the enum or pointer and a 32-bit integer. That forces it to occupy 32 bits with the proper alignment. When you read or write it on the 32-bit side, it'll see a properly aligned and sized 32-bit entity. When you read or write it on the 16-bit side, it will see a 16-bit entity.
  • You don't understand the problem. Please reproduce the problem your self. Or forward it to a more experiences TI employee.

    The problem is not in the CLA but in the main program.

     I will show you;

    CLA mem: enum is int32.

    Cla1ToCpuMsgRAM  enum is int32

    in main memory enum is int16.

    When you copy enums in CLA: in32=int32 // which is correct!

    When you copy/define a enum in main program with memory from Cla1ToCpuMsgRAM   the compiler assumes it is int16 so It typecast it to: int32=(int16)int32;

    So if there is any value(uninitialized) in the high part of the int32 your enum value is invalid. And that is a problem.

     To get around the int32=(int16)int32; typecast

     I solved it this way in the main program and not in the CLA!!

        long *ptr = (long *)&Servo_profile_init.state;
        *ptr=0;

    In this way the complete enum is completely cleared  in main memory. 

    It is a compiler issue because the size of a enum is not always int16 in main program. it is int32 when it is placed Cla1ToCpuMsgRAM so the compiler need to manage that.