Other Parts Discussed in Thread: CCSTUDIO
Hello,
I created a dynamic executable and i wanted to test it with a simple dynamic library. I follow the tuto that is describe in : 
. But i have a problem. When I want to build my dynamic library, i have : fatal error : could not open source file "stdio.h". I tried to add it in the current directory, and it did not work. I tried to add the path (with the cl6x compiler, option -i) to the library (which is in the include directory in CCS) and it did work even. I created a ccflag.cfg within there is only this : -i"D:\APP\TI\CCStudio_v5.5.0x86\ccsv5\tools\compiler\msp430_4.2.1\include". But it did not work. The only thing which worked is when i wrote : #include <D:\APP\TI\CCStudio_v5.5.0x86\ccsv5\tools\compiler\msp430_4.2.1\include\stdio.h>. But it did not find anothe header file; that mean i have to change all the files in the include directiry. It is too dangerous and it is not a clean method.
Can you help me please
PS : I put : cl6x -mv6740 -abi=eabi hello.c -z --dynamic=lib cmd_file=ccflag.cfg -o hello.elf oe.exe -entry_point=start into the windows terminal. I work on EVMC6748 DSP connect with a XDS510 USB on CCS v5_5
If you need more informations let me know. and sorry for my english.