This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error - The controller has detected a target power loss



Hi, there,


The "Test Connection" is passing without any errors, but I get following error message during connecting to target:

Error connecting to the target: (Error -180 @ 0x2A4C) The controller has detected a target power loss. The user must turn-on or connect the power supply for the target. (Emulation package 6.0.83.1)

I am using CCS6.1.0 with XDS100v3 emulator, the target is ARM7.

Any ideas?


Regards!

Wen

  • Hello,
    Note that you are using an older version of CCS and emulation package. I suggest updating both (Installing 6.1.3 would also update the emulation package). Also, what is the exact device you are using?

    Thanks
    ki