Other Parts Discussed in Thread: TM4C123GH6PM
compiler version : TI v15.12.1.LTS
Family : ARM
Varient : Tiva TM4C123GH6PM
When try to build c++ class in main.c It is giving below error
**** Build of configuration Debug__TI for project Lab1 **** "C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all 'Building file: ../Generic.cpp' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C123GH6PM --diag_wrap=off --diag_warning=225 --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="Generic.d" "../Generic.cpp" 'Finished building: ../Generic.cpp' ' ' 'Building file: ../main.c' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C123GH6PM --diag_wrap=off --diag_warning=225 --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="main.d" "../main.c" >> Compilation failure subdir_rules.mk:14: recipe for target 'main.obj' failed "..\Generic.h", line 11: error #20: identifier "class" is undefined "..\Generic.h", line 11: error #66: expected a ";" "..\Generic.h", line 15: warning #12-D: parsing restarts here after previous syntax error "../main.c", line 6: error #20: identifier "generic" is undefined 3 errors detected in the compilation of "../main.c". gmake: *** [main.obj] Error 1 'Building file: ../tm4c123gh6pm_startup_ccs.c' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" -g --gcc --define=ccs="ccs" --define=PART_TM4C123GH6PM --diag_wrap=off --diag_warning=225 --display_error_number --abi=eabi --preproc_with_compile --preproc_dependency="tm4c123gh6pm_startup_ccs.d" "../tm4c123gh6pm_startup_ccs.c" 'Finished building: ../tm4c123gh6pm_startup_ccs.c' ' ' gmake: Target 'all' not remade because of errors. **** Build Finished ****
class details are :
main.c
#include "Generic.h"
int main(void) {
Generic *generic;
return 0;
}
Generic.cpp
#include "Generic.h"
Generic::Generic() {
// TODO Auto-generated constructor stub
}
Generic::~Generic() {
// TODO Auto-generated destructor stub
}
Generic.h
#ifndef GENERIC_H_
#define GENERIC_H_
class Generic {
public:
Generic();
virtual ~Generic();
};
#endif /* GENERIC_H_ */
I am not sure whether we need to make main.c to main.cpp. If that is so then which make file need to updated for main.cpp
Any help on c++ compilation