Hi,
I am sampling some new NAND flash (Micron's MT29F8G08ABABA) to check compatibility with the DM365 & I am investigating my options re flashing. Currently my options are UART, Ethernet & JTAG. This post refers to my JTAG queries:
I have done some investigation into the available JTAGs and found that the XDS100v2 seems the most feasible (/cost effective) for my two tasks which are to 1) verify the integrity of the actual PCB (boundary scanning) & 2) the erase and program the NAND (UBL, uBoot, Kernel & FIlesystem). I am not interested in low level debugging at the moment. My questions are as follows:
- Is the XDS100v2 the guy for me to achieve the above tasks?
- Will I get away with doing the above tasks using the free unlicensed version of CCS4? I have read the that this free license is "limited" but cannot find out exactly what this limit implies ? Its not 'time' is it?
-Is it possible to use the XDS100v2 to perform the above tasks in a production (dos based) environment without using CCS?
-Is there anything worth considering when deciding where to buy it from ie Blackhawk vs TI vs any of the other manufacturers?
All input would be appreciated!
Sincerely,
NickA