This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 6.1.2 Adding driverlib to existing project not possible (MSP430FR6989)

Other Parts Discussed in Thread: MSP430FR6989

Hi,

i want to add the driverlib to an existing project.

The User Guide says:

"To add driver library to an existing project we recommend using CCS project templates. For driver library to work with project templates CCS must have discovered the driver library RTSC product. For more information refer to the installation steps of the release notes. CCS project templates adds the needed driver library source files and adds the driver library include path. To apply a project template right click on an existing project then go to Source -> Apply Project Template as seen in the screenshot below."

I installed the MSPWare 3.30.0.18 with the driverlib and it has been found by CCS and works when i create a new project.

But when i use an existing project (the same MSP is configured: MSP430FR6989) and go to Source -> Apply Project Template there is only the "FRAM Utilities Additions".

In the Preferences under Code Composer Studio -> RTSC -> Products the Driverlib is correctly shown:

It doesn't work when i create a new project for this MSP and try to add the driverlib later too.

I have installed the MSPWare to C:/ti and the CCS6.1.2 to c:/ti_ccs_v6.1.2. Could this be a problem? I guess not because it works for new projects, but who knows.

Regards

Sebastian