This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

After stop build project, CCS 6.1 doesn't work anymore

Hi everyone,

 

I’m using CCS 6.1 and no problems were found…until now. When my project was being built, I stopped it, and since then, the project never is built. I can make mistakes into the code, and no problems are found.

 

The console window shows as follow:

 

**** Build of configuration Flash for project PCB_Motor ****

 

"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all

 

**** Build Finished ****

 

It can be very weird, but this behavior only happens in one Workspace. The rest are working fine. Could you kindly give me any advice?

Thank you in advance.