Other Parts Discussed in Thread: OMAP-L137
Hi there,
I am using OMAP-L137/C6747 Eval board with CCS v3.3. It is working find and I am able to run all the examples but I want to use TI-RTOS and NDK tools and I think it would be good to use the latest CCS v6. So after installing CCS and when I tried to add XDC tools 3.10.5.61 I am getting an error.
Now, I am not sure if I have to still use the old version of the XDC tool if so how can I fix it?
Operation details
Cannot complete the install because one or more required items could not be found.
Software being installed: RTSC/XDCtools 3.10.5.61 (org.eclipse.rtsc.xdctools.feature.group 3.10.5.61)
Missing requirement: Model Plug-in 3.10.5.61 (org.eclipse.rtsc.xdctools.model 3.10.5.61) requires 'bundle org.eclipse.pde.runtime 0.0.0' but it could not be found
Cannot satisfy dependency:
From: RTSC/XDCtools 3.10.5.61 (org.eclipse.rtsc.xdctools.feature.group 3.10.5.61)
To: org.eclipse.rtsc.xdctools.model [3.10.5.61]
I did install the latest version of the XDC tools 3.32.00.06 but then I am not able to target OMAP-L137 or build example related to OMAP-L137.
Could someone please help me with this. Thanks.
Regards,
Mitesh