Other Parts Discussed in Thread: CONTROLSUITE
sir
i am beginner. i am using example build setting from v15c iq_math library and it gives error. when i use same example than also.
error is:
Description Resource Path Location Type
#10010 errors encountered during linking; "28335_IQsampleC.out" not built 28335_IQsampleC C/C++ Problem
<a href="file:/c:/ti/ccsv6/tools/compiler/dmed/HTML/10099.html">#10099-D</a> program will not fit into available memory. run placement with alignment/blocking fails for section ".esysmem" size 0x7d0 page 1. Available memory ranges: 28335_IQmath_lnk.cmd /28335_IQsampleC line 104 C/C++ Problem
gmake: *** [28335_IQsampleC.out] Error 1 28335_IQsampleC C/C++ Problem
gmake: Target 'all' not remade because of errors. 28335_IQsampleC C/C++ Problem
#10063-D entry-point symbol other than "_c_int00" specified: "code_start" 28335_IQsampleC C/C++ Problem
#16002-D build attribute vendor section TI missing in "C:/tidcs/c28/IQmath/v15a/lib/IQmath_fpu32.lib<atoIQN.obj>": compatibility cannot be determined 28335_IQsampleC C/C++ Problem
#16002-D build attribute vendor section TI missing in "C:/tidcs/c28/IQmath/v15a/lib/IQmath_fpu32.lib<IQ24atan2PU.obj>": compatibility cannot be determined 28335_IQsampleC C/C++ Problem
#16002-D build attribute vendor section TI missing in "C:/tidcs/c28/IQmath/v15a/lib/IQmath_fpu32.lib<IQ24div.obj>": compatibility cannot be determined 28335_IQsampleC C/C++ Problem
#16002-D build attribute vendor section TI missing in "C:/tidcs/c28/IQmath/v15a/lib/IQmath_fpu32.lib<IQ24exp.obj>": compatibility cannot be determined 28335_IQsampleC C/C++ Problem
#16002-D build attribute vendor section TI missing in "C:/tidcs/c28/IQmath/v15a/lib/IQmath_fpu32.lib<IQ24mag.obj>": compatibility cannot be determined 28335_IQsampleC C/C++ Problem
#16002-D build attribute vendor section TI missing in "C:/tidcs/c28/IQmath/v15a/lib/IQmath_fpu32.lib<IQ24mpyI32int.obj>": compatibility cannot be determined 28335_IQsampleC C/C++ Problem
#16002-D build attribute vendor section TI missing in "C:/tidcs/c28/IQmath/v15a/lib/IQmath_fpu32.lib<IQ24sin.obj>": compatibility cannot be determined 28335_IQsampleC C/C++ Problem
#16002-D build attribute vendor section TI missing in "C:/tidcs/c28/IQmath/v15a/lib/IQmath_fpu32.lib<IQmathTables.obj>": compatibility cannot be determined 28335_IQsampleC C/C++ Problem
#16002-D build attribute vendor section TI missing in "C:/tidcs/c28/IQmath/v15a/lib/IQmath_fpu32.lib<IQNexpTable.obj>": compatibility cannot be determined 28335_IQsampleC C/C++ Problem
Build variable 'XDAIS_CG_ROOT' cannot be resolved. 28335_IQsampleC properties Problems
Invalid project path: Include path not found (\packages\ti\xdais). 28335_IQsampleC pathentry Path Entry Problem
is there some problem in ccs or settings