This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems with TMDSHVMTRPFCKIT F28035 target connection

Hi all. I use 'Russian' as Regional setting (in hardware section of I was told to change decimal separator from comma to period in order to match en_US style) in Windows 7 x86 Ultimate, UAC on.

(1) Setup stage. Setup is displayed in "abracadabra" -- unreadable Eastern-European symbols. I had to switch to English before setup. Will this issue be fixed in some of next releases?

(2) After successful installation of CCS4 (comes with a Kit; I had to Uninstall CCS due to Update errors (I have forgotten to switch language back to English and cancelled setup, but no updates are shown now -- I'll have to start from scratch) and after step-by-stepping in guide of running KITexample I'm getting error of connection to Target namely in CLA0 not in C28x.

In order to try some other points I've successfully connected (via changing target configuration) to separate F28335 docking station (I've not yet tried to insert F28035 into dock station -- all faults are while connected to KIT). Also CCSv3.3 successfully connects to KIT@F28035 but is unable to do anything since in popups with message about unsupported processor code.

Any recommendations to solve my problem?