Hi,
I'm assuming this is an easy fix for something I'm missing, I haven't played with uController for at least 3 years.
I have just received and now installed all the software for the CC1310DK, and I can't get CC to connect and debug the board. Smart RF Studio, SmartRF Flash all find the board no worries, CC doesn't
The error message I get is:
Error connecting to the target:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.
(Emulation package 6.0.222.0)
That doesn't particularly make sense to myself since the board is new so the firmware should be good, and the other programs don't seem to have an issue.
Details:
- CC = v6.1.3.00033
- Windows 8.1
- CC1310DK, board for debug is SmartRF06
My guess is there i some link the background I must set to CC. CC was installed tot he default c:\ti space, the others to their default c:\programs files(x86)\Texas Instruments\..
Best Regards,